AI Can Code Now
What That Means for Tech Jobs
Image Source:
monsitj/Stock.adobe.com
By Becks Simpson for Mouser Electronics
Published October 6, 2022
Although software is supposedly “eating the world,” it is heavily restricted in doing so by access to
development talent and the increasing number of tasks required to build software. The number of jobs requiring
software developers is increasing at a rate that vastly outpaces the number of skilled professionals entering
the market to fill those roles. Even for those already in a programmer role, most of their time is not
necessarily spent coding new features but rather writing tests, patching security issues, reviewing code, and
fixing bugs. These two factors make it even more important to boost the productivity of those in the workforce,
and the most recent improvements in AI-driven natural language processing (NLP) models are making that a
reality. By virtue of their size, underlying architecture, and training data and regime, the newest generation
of state-of-the-art NLP models—called generative pre-trained transformers (GPTs)—can translate
between many languages, including from text to code. Embedding this powerful ability into tools that developers
can use is already proving invaluable at making developers better at their jobs and unlocking software
production for less technical folks.
Software Struggles to Eat the World
Along with the explosion of software for all sorts of use cases and business applications in the past decade
plus, an equivalent has emerged for the number of jobs that require coding experience to build that software. A
survey by Code.org in 2017 showed an estimated 500,000 open programming roles available in the United States
alone, but unfortunately, many go unfilled, especially since only 43,000 computer science graduates enter the
market every year, a figure that has decreased in recent years. On top of that, the time usually taken to become
skilled enough to take those jobs ranges from 3 to 5 years; by the time a programmer is ready to enter a more
senior role, the number of available roles will have increased by 28% (U.S. Bureau of Labor Statistics). As
such, the bottleneck of talent stymies many companies’ attempts to build impactful software.
Once a team of developers is in place within a company, the challenges don’t stop. Requirements for
building software, particularly in terms of quality, security, and speed of delivery, are increasingly complex.
Surprisingly, developers will spend only about 30%–40% of their time developing new features or improving
existing code (Newstack). This is because a large portion of their work also includes writing tests, making
fixes, and solving security issues. Senior developers will also spend a portion of their time mentoring the
juniors on their team and performing code reviews. All of these elements combined can impact delivery speed and
cost-effectiveness of a software project. It also provides the perfect opportunity to pair AI with human
developers to help address a lot of these drawbacks.
AI + Developers = Pair Programming Dream Team
AI-driven Coder Tools
With the strides that deep learning–based NLP has made in the past couple of years, a number of tools have
emerged with AI at their core, designed to improve the productivity and code quality of developers. In
particular, the models that these tools use can parse code to identify bugs and flaws, effectively performing
some of the more tedious parts of a code review. A few such tools released recently, like CodeGuru and DeepCode,
were able to find vulnerabilities that were difficult for humans to identify as well as find that 50% of the
pull requests studied had issues (AI-News).
Figure 1: The architecture of Copilot showing how GitHub uses Codex under
the hood to provide code suggestions
and write software fragments. (Source: https://copilot.github.com/)
Additionally, modern NLP techniques improve developers' code quality and speed up development by helping
auto-complete sections of code, monitor their code output for errors, and even auto-generate unit tests.
OpenAI’s Codex algorithm, which was incorporated into GitHub’s Copilot, can do this with astounding
accuracy, even going so far as to generate code from human language input (Figure 1). Its
ability to do this comes from the data it was trained with, both natural language fragments and a vast amount of
code. A preliminary study from GitHub on its performance showed that for a mundane task like writing an HTTP
server, leveraging AI alongside a developer reduced time to completion by half. The fact that the model
underpinning this tool can auto-complete entire code sections from a single comment also makes coding vastly
more accessible to beginners and less technical folks.
Coding Made More Accessible
The powerful AI translation capabilities of this new generation of NLP models means that, within some limits,
anyone can use human language to produce snippets of code that they need. These pieces of software can be in any
programming language as well, from those used to execute certain routines like Python, JavaScript, and C++ to
those used to access data in various databases like SQL and NoSQL. Provided that the program a person would like
to code is not overly complicated, tools like Codex can likely help. It has proven useful for making small
websites, deriving excel functions, and converting what a user would like from human language to the query
language used to access the data. However, as the researchers of these techniques note, the models are not
totally correct all the time. Often, the code produced is mostly correct but requires some intervention from an
experienced developer. In this sense, the models can boost the productivity of a human coding tutor in that they
can take over where the AI runs into issues as it is being used by a less experienced person. This can also mean
that junior developers’ productivity is greatly increased while their requirement for supervision and
senior input is reduced.
From Human Language to Computer Language
So how do most of these tools work? The main workhorse powering these innovative tools is the GPT—typically
the third generation of such models, called GPT-3. This architecture was initially developed by OpenAI and
trained on a massive amount of text from across the internet, including prose, digital books, tweets,
open-source repositories, comments, online articles, and more. Although the goal was always more realistic
language generation, the side effect of the model also being able to generate code led to the later development
of Codex.
Several factors separate GPT generations from previous deep learning–based NLP models. These include the
amount of data used for training and the way in which the models were trained as well as the number of
parameters the models have and their state-of-the-art underlying architecture. Since these models and their
predecessors are neural networks, the number of parameters influences the complexity of relationships in data
that they can capture, meaning that bigger models can learn more nuanced patterns than smaller models. These
models were also trained in a multitask setting and in a self-supervised fashion. Most neural networks are made
to perform a single task and as such take specifically-labeled data in order to learn how to do that
task—a great example being AlphaGo, which is great at GO but cannot play chess. Requiring labeled data is
called supervised learning. The GPT-3, by contrast, was trained to predict the next word in a sequence, so the
data don’t need labeling; this is the backbone of many tasks like translation, text generation, and
question answering.
Figure 2: A visualization of the attention mechanism, or which words the
model focuses on when considering the
current word. (Source: Ketan Doshi / Towards Data Science Blog)
Additionally, there are transformer models, which perform better than previous NLP benchmarks like long
short-term memory models or recurrent neural networks. They process entire sentences at once instead of word by
word, store and use similarity scores between words in a mechanism called “attention,” and encode
information related to a specific position of a token in a sentence (Figure 2). All of this
allows for a bigger model that can learn more since parallelization and recursion are no longer issues, as they
were in the past. It also removes the difficulties previous models had with forgetting relationships between
far-apart words and sentences. Since the GPT-3 is available through an application programming interface
provided by OpenAI, it can be incorporated into other AI for coding products, which democratizes access to
coding even further.
Conclusion
In order to continue building the vast amount of software needed to cover all the applications that require it,
AI is stepping in to help boost the productivity of developers. Since the demand for programmers clearly
outstrips the supply, leveraging other solutions to augment the output and code quality of coders companies
already have is proving more and more beneficial. With the recent dramatic improvements in AI-based NLP models,
such as the particularly powerful GPT-3, the dream of an AI-powered pair programmer for human developers is
becoming a reality. With such models embedded in their everyday tools, programmers can stand to gain a lot in
terms of reduced time spent on repetitive tasks like writing tests and improved code quality from automated
reviews and auto-generated snippets. Even junior developers and less technical folks can benefit from the
text-to-code capabilities now available. Software may not be able to eat the world alone, but AI can certainly
help.
Author Bio
Becks is a technical
lead for machine learning at Imagia, a Montreal-based startup putting AI in the hands of clinicians to drive
medical research. In her spare time, she also works with Whale Seeker, another startup using AI to detect whales
so that industry and these gentle giants can coexist profitably. She has worked across the spectrum in deep
learning and machine learning from investigating novel deep learning methods and applying research directly for
solving real world problems to architecting pipelines and platforms to train and deploy AI models in the wild
and advising startups on their AI and data strategies.